Stay informed

Optimierte Reinraumfertigung: Neuer Produktionsbereich von Maximator

Maximator creates a new production area – for optimised cleanroom production

How item assisted in creating a new ISO 6 cleanroom for the semiconductor industry.

Maximator GmbH is a leading light in high-pressure technology, boasting more than 40 years of experience in developing and building components and systems for numerous industries and applications. More than 400 skilled employees are based at the company’s headquarters in Nordhausen, Germany, while sales offices throughout the country and partner companies worldwide help customers find solutions containing high-pressure technology, hydraulics and pneumatics.

In February 2026, Maximator put a new cleanroom into operation at its Nordhausen location, expanding its cleanroom production facilities with a specific focus on customer projects that require exceptionally high cleanliness standards and extremely reliable processes. This controlled environment is where Maximator produces gas compressor systems for customer projects in the semiconductor industry. The new production area was created using modular cleanroom technology from item.

Cleanroom solutions in action

Want to see machine cabins with air current visualisation or walk-in cleanrooms? Come and visit the item cleanroom center in Solingen. Simply fill in our contact form and we’ll get back to you to arrange a date as soon as we can.

SIGN UP NOW

A cleanroom project on a large scale

It took just four months or so to build an ISO 6-compliant cleanroom with a floor area of 70 m² and a volume of 175 m³. The construction work used around 2 km of profile material, 1000 fasteners and 183 m² of panel elements in total, resulting in a cleanroom structure weighing in at 3.6 tonnes overall. At a sum in the region of 250,000 euros, this investment has laid the groundwork for strengthening Maximator’s expertise in producing ultra-clean high-pressure components and systems.

“item was a supportive partner and transparent in the information it shared with us, something for which we’re very grateful. It gave us specific recommendations about requirements to fulfil and how to go about execution, allowing us to set the right course for the cleanroom project early on and complete it in line with our goals,” says Dr Alexander Müller, Managing Director at Maximator.

From cleanroom tent to walk-in cleanroom

A long-standing item customer, Maximator started out by using our lean production products. This new project began in January 2025 and was sparked by the idea of creating a cleanroom tent; however, as planning continued, Maximator ultimately decided to build an entire cleanroom. The new concept was discussed in detail during meetings at the location.

A key advantage of the item Building Kit System is that it allows all solutions to adapt flexibly to new requirements and concept changes.

These revealed a key advantage of the item Building Kit System in that it would allow all solutions to adapt flexibly to new requirements and concept changes. After seeing initial proposals, including example solutions, and visiting the item cleanroom center in Solingen – where a VR headset also came into play – Maximator had a vivid impression of what its cleanroom plans could result in.

From the outset, the project included a clear list of requirements that the new cleanroom production facility had to meet: minimal risk of particles – and, therefore, contamination – getting in, reproducible production processes and optimised process strategies to ensure exceptional cleanliness and precision. With so many of the customer’s departments involved in this complex project, a weekly meeting was held to hear everyone’s views.

item also organised a workshop in Mühlhausen that gave Maximator project managers and trainees the opportunity to learn practical skills for building cleanroom components. The trainees were able to put their freshly acquired knowledge directly into practice and, alongside the factory equipment construction team, played a significant part in building the cleanroom.

Modular infrastructure for cleanroom production

The new cleanroom comprises a production space of around 60 m² plus areas for technical services and for moving around. It is divided into three zones – non-clean, clean and ultra-clean – and a manually monitored pressure cascade concept of around 30 pascals (Pa) keeps the structure running efficiently. Pressure differentials are created between the zones so that air flows from the cleaner zones to the less clean ones, preventing particles from getting into critical areas.

Personnel and material airlocks provide controlled transition points, acting as buffers between cleanliness levels and keeping processes regulated when staff changeovers take place or material is being picked, for example. They also prevent direct exchange of air and particles between non-clean and ultra-clean areas when doors are opened. The result is that conditions are kept stable and reproducible to accommodate sensitive process steps.

The new cleanroom now means that our production facilities include ultra-modern infrastructure.

The cleanroom production facility meets the requirements of ISO class 6 as specified by ISO 14644-1. At the same time, the design means that it will be possible to use the space for installing and signing off other high-pressure assemblies and components in the future, including pumps and valves, for example. “The new cleanroom now means that our production facilities include ultra-modern infrastructure that will help us fulfil customer requirements, even demanding ones, with consistently high standards of quality – plus reliable processes and guaranteed low particle levels,” states Dr Alexander Müller.

The new ISO 6 cleanroom at Maximator, featuring assembly workstations
A look at the new ISO 6 cleanroom at Maximator, featuring assembly workstations.

Constructing the cleanroom with the item Building Kit System

The cleanroom structure uses numerous components from our item Building Kit System. It is based on Line X 8 profiles and the Fixing System for panels, while the ceiling construction uses the Profile X 8 240×40 1NO. With its combination of a high section modulus and low dead weight, this profile is particularly suitable for adding rigidity to self-supporting ceilings.

Other item components used in the structure are:

The Access Doors reliably separate working areas and can be used from both sides. Featuring an all-round seal, they are available as standardised products or can be configured to suit individual requirements. The Adjustable Feet come with a stepless height adjustment mechanism and keep installations stable.

The FFUs filter the room air and produce an adjustable laminar displacement airflow. Meanwhile, the Drop-In Light Fittings distribute light evenly and without glare across large working areas. They are integrated directly into cleanroom grid ceilings using the Fixing System.

Wall trunking allows cabling to be installed tidily within the wall – an approach that is compatible with cleanrooms – and its bevelled surfaces help prevent particle deposits. There are also Multi-Segment RGB LED Strips to keep everything happening in the production facility clear to see. Not only that, but the new cleanroom has incorporated all the products from the range of item new products for 2025.

Cleanroom production facility for controlled production conditions and flexible adaptations
The new cleanroom production facility maintains controlled production conditions and can be flexibly adapted to suit different requirements.

New possibilities for high-tech sectors

The new ISO 6-compliant cleanroom is allowing Maximator to expand its production capabilities beyond just the semiconductor industry: the infrastructure has also established a foundation for more growth in demanding sectors with a viable future ahead of them, such as medical technology, food technology, pharmaceutical technology, biotech and aerospace.

With the ISO 6 cleanroom, Maximator is strengthening its position in numerous high‑tech industries – far beyond its existing markets.

As a result, the modular item building kit principle has made it possible to create a solution that not only meets the needs of today’s cleanroom production environments, but is also adaptable: “With the ISO 6 cleanroom, Maximator is strengthening its position in numerous high‑tech industries – far beyond its existing markets. Wherever it is vital to ensure low particle levels and reliable processes and functions, an ISO 6‑compliant assembly process makes it possible to achieve proven quality standards efficiently while cutting down on costs and the work involved in processes,” explains project manager Andor Thelen.

Are you interested in cleanroom solutions? Then we have something that’s right up your street! Simply subscribe to the item blog by completing the box at the top right.